This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F280048C-Q1: 关于TMS320F280048C芯片引导模式选择和CMPSS模块比对输入的问题?

Part Number: TMS320F280048C-Q1


1、对于这款芯片的引导模式选择引脚GPIO24和GPIO32,GPIO32这个引脚是否可以同时复用为CANA_TX功能?

2、对于这款芯片,如果要用内部CMPSS模块,CMPSS模块的输入是否能与模拟量输入功能同时用,也即模拟量输入的同时也是CMPSS模块外部比对的输入信号?如果不是该怎么处理?

  • 1、可以,上电/复位的时候确保boot引脚电位就可以,完成上电/复位之后就可以释放引脚。一般可以用外部弱上/下拉的方式来处理

    2、可以同时使用,内部是联通的。

  • 好的,谢谢Green Deng 。顺便还有个如下问题请教:

    1、如果芯片用外部1.2V供电,GPIO22_VFBSW和GPIO23_VSW引脚可否做普通GPIO口用?

    2、如果芯片启用内部CMPSS模块做模拟比对,用内部的可编程参考12位DAC驱动做比对的负向参考电压,此时GPIO22_VFBSW和GPIO23_VSW引脚状态如何,是否还可以用于普通GPIO口?

  • 1、可以。这点datasheet上写的应该挺清楚的

    If the internal DC-DC regulator is not used, this can be configured as General-Purpose Input Output 22 by disabling DC-DC and clearing their bits in GPAAMSEL register.

    2、不好意思这里我没看明白你的问题。我的理解,只要没有使用内部DC-DC的话就可以配置为GPIO。使用内部DC-DC的话这两个引脚会被配置为VFBSW和VSW

  •  ,你好!我的意思是CMPSS模块启用内部12位DAC参考,不会影响GPIO22_VFBSW和GPIO23_VSW引脚的应用吧?

  • 我大致浏览了一下芯片TRM,没有找到这方面的说明会影响这两个引脚的使用。

    查找了一下中英文E2E论坛,也没有相关的帖子讨论这两者的使用的