This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28035: 使用无源晶振时X2管脚对外输出3.3V时钟方案咨询

Part Number: TMS320F28035

28035使用10M无源晶振,接在X1和X2之间,目前硬件设计想把这个10M晶振的时钟引出,接入FPGA,作为FPGA的时钟输入。目的是使FPGA和28035之间时钟同步。

因为FPGA的电平为3.3V,28035片上振荡器为1.8V,需要把1.8V转换为3.3V电平,初步计划使用74LVC1T45作为1.8V转3.3V芯片,同时由于板上没有1.8V电源,希望使用28035的54脚片上LDO输出的1.8V作为74LVC1T45的1.8V供电,请问该方案是否可行,或者有没有其它更好的方案。

ps.XCLKOUT管脚已经占用,无法作为时钟输出。