Part Number: F28M35H52C
原来uart收发采用中断的方式实现,嫌中断太频繁,现在想改dma,使用的串口1,用的是udma_demo,只开了uart发送的dma,接收部分以及ram to ram部分注释掉了,我理解udma配置好了,通道使能就可以发送了,需要其他操作吧,使能部分我尝试读了,都是faulse
代码flash运行,管脚配置正确,时钟都正确*(单测试串口发送可以用测试代码发送数据到上位机显示。)
大致过程参考了demo,同时对着spru22i手册查看了16.4.3部分寄存器的设置,
代码 如下:
void UART1IntHandler(void)
{
unsigned long ulStatus;
ulStatus = UARTIntStatus(UART1_BASE, 1);
UARTIntClear(UART1_BASE, ulStatus);
if(!uDMAChannelIsEnabled(UDMA_CHANNEL_UART1TX))
{
uDMAChannelTransferSet(UDMA_CHANNEL_UART1TX | UDMA_PRI_SELECT,
UDMA_MODE_BASIC, g_ucTxBuf,
(void *)(UART1_BASE + UART_O_DR),
sizeof(g_ucTxBuf));
// The uDMA TX channel must be re-enabled.
uDMAChannelEnable(UDMA_CHANNEL_UART1TX);
/////// 怎么读都是没有使能
// uDMAChannelIsEnabled(UDMA_CHANNEL_UART1TX);
}
}
//*****************************************************************************
void
InitUART1Transfer(void)
{
unsigned int uIdx;
for(uIdx = 0; uIdx < UART_TXBUF_SIZE; uIdx++)
{
g_ucTxBuf[uIdx] = uIdx;
}
SysCtlPeripheralEnable(SYSCTL_PERIPH_UART1);
SysCtlPeripheralSleepEnable(SYSCTL_PERIPH_UART1);
UARTConfigSetExpClk(UART1_BASE, SysCtlClockGet(SYSTEM_CLOCK_SPEED), 115200,
UART_CONFIG_WLEN_8 | UART_CONFIG_STOP_ONE |
UART_CONFIG_PAR_NONE);
UARTFIFOLevelSet(UART1_BASE, UART_FIFO_TX4_8, UART_FIFO_RX4_8);
UARTEnable(UART1_BASE);
UARTDMAEnable(UART1_BASE, UART_DMA_TX);
IntEnable(INT_UART1);
uDMAChannelAttributeDisable(UDMA_CHANNEL_UART1TX,
UDMA_ATTR_ALTSELECT |
UDMA_ATTR_HIGH_PRIORITY | UDMA_ATTR_REQMASK);
uDMAChannelAttributeEnable(UDMA_CHANNEL_UART1TX, UDMA_ATTR_USEBURST);
uDMAChannelControlSet(UDMA_CHANNEL_UART1TX | UDMA_PRI_SELECT,
UDMA_SIZE_8 | UDMA_SRC_INC_8 | UDMA_DST_INC_NONE |
UDMA_ARB_4);
uDMAChannelTransferSet(UDMA_CHANNEL_UART1TX | UDMA_PRI_SELECT,
UDMA_MODE_BASIC, g_ucTxBuf,
(void *)(UART1_BASE + UART_O_DR),
sizeof(g_ucTxBuf));
////测试串口配置,管脚是否正确,能接到计算机上正常收到数据
// UARTCharPutNonBlocking(UART1_BASE,0xaa);
// UARTCharPutNonBlocking(UART1_BASE,0xaa);
// UARTCharPutNonBlocking(UART1_BASE,0xaa);
// UARTCharPutNonBlocking(UART1_BASE,0xaa);
// UARTCharPutNonBlocking(UART1_BASE,0xaa);
uDMAChannelEnable(UDMA_CHANNEL_UART1TX);
}
int main(void)
{
HWREG(SYSCTL_MWRALLOW) = 0xA5A5A5A5;
// Sets up PLL, M3 running at 75MHz and C28 running at 150MHz
SysCtlClockConfigSet(SYSCTL_USE_PLL | (SYSCTL_SPLLIMULT_M & 0xF) |
SYSCTL_SYSDIV_1 | SYSCTL_M3SSDIV_2 |
SYSCTL_XCLKDIV_4);
#ifdef _FLASH
memcpy(&RamfuncsRunStart, &RamfuncsLoadStart, (size_t)&RamfuncsLoadSize);
FlashInit();
#endif
////配置管脚
PinoutSet();
// Disable clock supply for the watchdog modules
SysCtlPeripheralDisable(SYSCTL_PERIPH_WDOG1);
SysCtlPeripheralDisable(SYSCTL_PERIPH_WDOG0);
// Unlock the register to change the commit register value for Port B Pin 7
// This disables the NMI functionality on the pin and allows other muxing
// options to be used
HWREG(GPIO_PORTB_BASE+GPIO_O_LOCK) = GPIO_LOCK_KEY_DD;
// Write to commit register
HWREG(GPIO_PORTB_BASE+GPIO_O_CR) |= 0x000000FF;
// Delay
for (i=0;i<20;i++){};
// Enable peripherals to operate when CPU is in sleep.
SysCtlPeripheralClockGating(true);
// Register interrupt handlers in the RAM vector table
IntRegister(INT_UART1, UART1IntHandler);
// Enable the uDMA controller at the system level. Enable it to continue
// to run while the processor is in sleep.
SysCtlPeripheralEnable(SYSCTL_PERIPH_UDMA);
SysCtlPeripheralSleepEnable(SYSCTL_PERIPH_UDMA);
// Enable the uDMA controller error interrupt. This interrupt will occur
// if there is a bus error during a transfer.
IntEnable(INT_UDMAERR);
// Enable the uDMA controller.
uDMAEnable();
// Point at the control table to use for channel control structures.
uDMAControlBaseSet(ucControlTable);
// Initialize the uDMA UART transfers.
InitUART1Transfer();
// Loop until the button is pressed. The processor is put to sleep
// in this loop so that CPU utilization can be measured.
while(1)
{
;
}