This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F2806的烧写问题



35块板子,第一次烧写,全部烧写正确,第二次烧写有11块烧写错误,程序一样,电路一样(可以排除虚焊状态)。我用的是CCS5.3,在CCS环境下烧写,芯片“Test Connection”正确,如果只Load progran是正确的,但只要erase就不正确了?无密码定义。

电压3.3V、内部1.9V、XRS信号、CLK输入都正确!Cmd 文件检查也正确。

第一次烧写完成后,板子经过了50度的高温老化,8个小时时间,芯片温度55度左右。难道高温把Flash损坏了?

烧写错误后出现以下提示:

C28xx: Flash operation timed out waiting for the algorithm to complete. Operation cancelled.
C28xx: GEL: File: D:\tmp\temp.out: Load failed.

以前调试时从未出现此现象,板子多了就出现这个问题了。请教哪位大虾帮忙分析一下,谢谢!