This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F280049: GPIO的输入滤波问题

Part Number: TMS320F280049


各位大神好,请教一个问题,我用qep去接收外部脉冲信号,为了应对外界可能存在的干扰,我想引入管脚滤波。

但是看起来只能用管脚的GPIO滤波,也就是去设置

GpioCtrlRegs.GPACTRL.bit.QUALPRD0~QUALPRD4,但是每个寄存器对应8个GPIO

还有 GPAQSEL1, GPAQSEL2, GPBQSEL1, and GPBQSEL2  这几个寄存器去配置多次采样。

在100M主频的情况下,设置QUALPRD为255,GPxQSEL选择6次采样,那这样最慢的频率也就是100M/2/255/5=39.2K,因此有以下问题:

如果我设置的GPIO区间,同时包含SPI等高速信号,会不会造成冲突,导致SPI等高速信号接口异常