This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
请教各位 我使用f28027F跑 InstaSPIN-FOC 运行Lab02b辨识程序是 电机在EST_State_RatedFlux识别磁通时运行FluxWaitTime[EST_Flux_State_CL1]10秒后 电机停止,然后运行到EST_State_Ls是 电机微弱摆动,结束后Ls识别值为1.8...........。我这边开始增加USER_MOTOR_FLUX_EST_FREQ_Hz 但是怎么改都无意义。请教这种情况是什么问题啊。在EST_State_RampUp状态是电机也能平滑的转动
你好呀,请问是在自己设计制作的PCB上做测试吗?是初次测试还是有测试成功过?
另外,几个lab都有说明,是否有参考user's guide对软硬件进行设置?
C:/ti/motorware/motorware_1_01_00_18/docs/labs/instaspin_labs.pdf
你好,我是用自己设计板子进行测试,驱动芯片MP6540A。初次测试。根据InstaSPIN-FOC user guide_CHN这个文档修改了很多user.h参数,测试下来现象都是一样的。在运行Lab02b时感觉电阻辨识都是错的辨识出来的Rs很小0.021118395.这时候我开始增加 pUserParams->RsWaitTime[EST_Rs_State_Fine]时间,这时候辨识出来的电阻直接就饱和了,出现了一个很大的值。然后我这边电流采集的方案是INA240A1PWR 采样电阻0.01R。电机功率是60W ,4000转左右。请问下我这边应该需要往那个方向进行排查。
这个可能要麻烦你前往英文E2E论坛咨询了,相对来说我们这边对套件比较熟悉,如果是其他硬件,最好联系一下英文论坛上专门负责电机控制的工程师来为你解答:e2e.ti.com/.../c2000-microcontrollers-forum