Other Parts Discussed in Thread: ADS131E06
我把28335对ADS131E06的读ID的时序说明一下:START脚下拉,保证一上电时,ADS131E06不转换,上电后,在仿真状态下,LOAD程序,然后准备仿真程序(这几步离上电已经超过至少10S)。在程序中,先对START脚拉低处理,然后发送ADS131的复位序列,之后等待一段时间(手册上要求18tclk以上,实际我们保证此时间远大于要求时间),然后发送读ID的命令序列(0x20 0x00),然后按照要求,等待至少4tclk时间,再发送8bit的SCLK,但始终是读不到ADS131的ID,监视到MISO口线上一直是低电平,不知道是什么问题。SCLK速率目前设置在2.88MHz左右,SPI口的时序也按照ADS131的要求配置了,我把复位及SPI读ID的波形图发上来,请大虾们帮忙看看,谢谢。