Part Number: TMS320F28377D
TI的 FAE您好!
我在28377D的CPU2的CLA进行一个数据的大小比较,编译提出了警告。不知道怎么处理。麻烦给点提示,代码如下:
在外部的c文件里定义一个数组
#pragma DATA_SECTION(u32DataCLAToCPU2,"Cla1ToCpuMsgRAM")
uint32_t u32DataCLAToCPU2[20];
CLA的代码如下
//Task 1 : Matrix multiply
__interrupt void Cla1Task1 ( void )
{
u32DataCLAToCPU2[0] += 3;
if(u32DataCLAToCPU2[0] >= 30000)
u32DataCLAToCPU2[0] = 0;
}
编译的提示如下:
"../matrix_mpy.cla", line 107: warning #30013-D: Comparison operation uses integer comparison instruction, which does not operate properly for values that would overflow subtraction. Use --cla_signed_compare_workaround=on to have the compiler work around this issue.
不知道该怎么处理这个问题