串口调试时,我利用串口助手自动发送获得响应
但随时间运行一段时间后我发现程序不再响应了,我的主程序的运行灯也不再工作,但用示波器测得硬件PWM是正常输出的
我的串口初始化函数为:
void HAL_setupSCI(void) { // // GPIO28 is the SCI Rx pin. // GPIO_setPinConfig(DEVICE_GPIO_CFG_SCIRXDA); GPIO_setDirectionMode(DEVICE_GPIO_PIN_SCIRXDA, GPIO_DIR_MODE_IN); GPIO_setPadConfig(DEVICE_GPIO_PIN_SCIRXDA, GPIO_PIN_TYPE_STD); GPIO_setQualificationMode(DEVICE_GPIO_PIN_SCIRXDA, GPIO_QUAL_ASYNC); // // GPIO29 is the SCI Tx pin. // GPIO_setPinConfig(DEVICE_GPIO_CFG_SCITXDA); GPIO_setDirectionMode(DEVICE_GPIO_PIN_SCITXDA, GPIO_DIR_MODE_OUT); GPIO_setPadConfig(DEVICE_GPIO_PIN_SCITXDA, GPIO_PIN_TYPE_STD); GPIO_setQualificationMode(DEVICE_GPIO_PIN_SCITXDA, GPIO_QUAL_ASYNC); // // 配置中断服务函数 // Interrupt_register(INT_SCIA_RX, &sciaRxISR); // // 初始化SCIA和它的FIFO // SCI_performSoftwareReset(SCIA_BASE); // // 50000000 is the LSPCLK or the Clock used for the SCI Module // 57600 is the Baudrate desired of the SCI module // 1 stop bit, No parity, 8 char bits, // SCI_setConfig(SCIA_BASE, LSPCLK_FREQ_H, 38400, (SCI_CONFIG_WLEN_8 | SCI_CONFIG_STOP_ONE | SCI_CONFIG_PAR_NONE)); // //No loopback // SCI_disableLoopback(SCIA_BASE); SCI_resetChannels(SCIA_BASE); SCI_resetRxFIFO(SCIA_BASE); SCI_clearInterruptStatus(SCIA_BASE,SCI_INT_RXFF); SCI_enableFIFO(SCIA_BASE); SCI_enableModule(SCIA_BASE); SCI_performSoftwareReset(SCIA_BASE); // // Set the transmit FIFO level to 0 and the receive FIFO level to 2. // Enable the TXFF and RXFF interrupts. // SCI_setFIFOInterruptLevel(SCIA_BASE, SCI_FIFO_TX0, SCI_FIFO_RX1); SCI_enableInterrupt(SCIA_BASE,SCI_INT_RXFF); // // Clear the SCI interrupts before enabling them. // SCI_clearInterruptStatus(SCIA_BASE,SCI_INT_RXFF); // // Enable the interrupts in the PIE: Group 9 interrupts 1 & 2. // Interrupt_enable(INT_SCIA_RX); Interrupt_clearACKGroup(INTERRUPT_ACK_GROUP9); }
接收中断函数为:
interrupt void sciaRxISR(void) { // // Read characters from the FIFO. // // SciRxBuf[SciRxPointHead] = SCI_readCharBlockingFIFO(SCIA_BASE); SciRxBuf[SciRxPointHead] = SCI_readCharNonBlocking(SCIA_BASE); SciRxPointHead ++; if (SciRxPointHead == RxLen) SciRxPointHead = 0; GPIO_togglePin(TTPLPFC_GPIO_LED1); // // Clear the SCI RXFF interrupt and acknowledge the PIE interrupt. // SCI_clearInterruptStatus(SCIA_BASE, SCI_INT_RXFF); Interrupt_clearACKGroup(INTERRUPT_ACK_GROUP9); }
发送函数为:
void SendMessageToSCI(uint32_t base, unsigned char *msg) { uint16_t msg_len = 0; while (msg[msg_len] != 0) { SciTxBuf[SciTxPointHead] = msg[msg_len]; SciTxPointHead ++; if (SciTxPointHead == TxLen) SciTxPointHead = 0; msg_len ++; } SCI_writeCharArray(base,(const uint16_t *)SciTxBuf,SciTxPointHead); SciTxPointEnd = SciTxPointHead = 0; memset(SciTxBuf,0,TxLen); }
不使用自动发送,缓慢调试时不会出问题,但是换成自动发送程序就会出错,请问是什么原因?