This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28062: 使用XDS110无法仿真

Part Number: TMS320F28062


-----[Print the reset-command software log-file]-----------------------------

This utility has selected a 100- or 510-class product.
This utility will load the adapter 'jioxds110.dll'.
The library build date was 'Jan 1 2021'.
The library build time was '11:25:57'.
The library package version is '9.3.0.00032'.
The library component version is '35.35.0.0'.
The controller does not use a programmable FPGA.

An error occurred while hard opening the controller.

-----[An error has occurred and this utility has aborted]--------------------

This error is generated by TI's USCIF driver or utilities.

The value is '-266' (0xfffffef6).
The title is 'SC_ERR_XDS110_CPLD_UPDATE'.

The explanation is:
An internal error occurred. The CPLD image update failed. Unplug and
re-plug the XDS110, and try again.

[End: Texas Instruments XDS110 USB Debug Probe_0]

已有驱动

可以仿真F280025,但不能仿真F28062,麻烦看下是什么问题,谢谢!