有没有6路TZ1~TZ6的dsp芯片?并且也有6路PWM1~PWM6的?不是很贵的那种。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好,首先要确认一下,你是要找C2000系列的MCU芯片吗?然后你说的“不是很贵的那种”,这个概念很主观啊,没办法具体给你定位。
如果是选择C2000的芯片,那都能满足每款芯片具有至少6个PWM模块,且每个模块都有一个TZ信号。相对来说性价比比较高的有F280021
额,这个表述不太正确,应该是每个PWM都被索引6个TZ信号了。如果要完成你提到的下面这种设置也是可以的
TZ1控制PWM1A,
TZ2控制PWM2A,
...
TZ6控制PWM6A。
具体的你可以看一下芯片TRM的17.9 Trip-Zone (TZ) Submodule
谢谢你的回复,我看了资料,TZ4~TZ6不是GPIO口引脚,而我需要的TZ1~TZ6是GPIO口引脚。
这样的话我印象中只有F28335是TZ1~6都索引到外部GPIO的