This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

请问一个关于TI套件问题



我买了一个TI的套件,现在在调试,其中TI提供的falsh可执行文件跟上位机都可以运行,现在我们利用controlsuit中源代码来自己改写,但是当我们直接编译controlsuit中的程序的时候是不可以直接运行的,我们的操作时lsw=0时电机定位到0°,然后将lsw=1此时电机开环运行(速度到了稳定),接着lsw=2那么电机进行闭环了,但是这个时候出现电机抖动一下或者直接过电流,而不是像TI提供的源码一样顺畅启动。

后来我分析看了说明文档,好像说先断开速度环,调节电流环并且开环启动,也就是先lsw=0,然后lsw=1,接着我们观察转子电角度,让smo的角度和rg模块的角度差不多,那这里我想知道是不是要调节SMO中的klide何kslf这两个参数呢,等调节好了,是不是就可以将接上速度环了呢?那PI参数一般是什么时候调节呢?

还有一个问题就是关于带传感器的,也是controlsuit中的HVPM_sersoned源码,我先想查出补偿角度的,但是我每次上电定位后出现qep第一次采样到的值都不一样的,而且有的时候我在电机不转的时候QEP的计数值还一直在变,不知道是什么原因!!

谢谢!!