This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

28335 烧Flash 时连接不上

Other Parts Discussed in Thread: UNIFLASH

网友jinpaidianzi在21ic TI DSP技术论坛问以下问题未能解决:

安装好ccs3.3后,设置中选择了 F28335 XDS510 Emulator    (我用的是仿真器usb2.0),设置好后连接成功,仿真操作一切正常。但是在SdConfig v3.3 软件中进行设置时,端口选择0x240时却没有XDS510选项,仅有spi510,RESET时失败。请问这种情况下是不是表示没有连接上?可是在CCS下进行仿真操作完全可以。

当烧Flash时,执行SDFlash.exe时还是无法复位。是不是仿真器不支持?

我注意到在SdConfig v3.3中端口0x510中对应XDS510USB,于是我就在SETUP CCS3.3中改配置为F28335 XDS510usb Emulator    ,可是却连接不上,请问这是什么原因?

  • 为什么会有这个问题,我看到CCSV3.3中XDS510USB 的USB Emulator  adress默认是0x510.

    通过CCSV3.3能够正常烧写芯片吗?

    SDFlash.exe是针对SDI公司的仿真器您用的是SDI的仿真器吗?

    如果不想用CCS烧写芯片,可以用TI的CCS_UniFlash来操作。另外也建议使用CCSV5。

    http://processors.wiki.ti.com/index.php/CCS_UniFlash_v2.1_Release_Notes

    CCSV5:

    http://processors.wiki.ti.com/index.php/Download_CCS