This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F280049: HRPWM 在up-down模式下的duty范围(TBPRDHR没有使能)

Part Number: TMS320F280049


F280049 TRM中关于HRPWM有提到存在Duty Cycle Range Limitationd的问题,当没有使能高分辨率周期(TBPRDHR)控制时,新周期开始后的三个EPWMCLK后开始启用。也就是每个周期开始的三个EPWMCLK是不能用的。如果采用up-count mode,就会存在最小占空比的限制,而采用down-count mode,就会存在最大占空比的限制。那如果是用up-down count mode产生对称波形,duty的限制是怎么样的呢?是最大最小duyt都会有限制吗?假设频率100kHz,duty的变换范围就是0.6%~99.4%?关于这个问题请专家帮忙看一下,希望能够收到回复,感谢!