This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

mp/mc引脚的作用



mp/mc引脚在高低电平时,DSP芯片处于什么工作状态

  • Microprocessor/Microcomputer     Mode     Select.  Switches  between microprocessor and microcomputer mode.

    When high, Zone 7 is enabled  on  the  external  interface.

    When  low,  Zone 7 is disabled from the external interface, and on-chip boot ROM may be accessed instead. This signal is latched into the XINTCNF2 register on a reset and the user can modify this bit in software. The state of the XMP/MC pin is ignored after reset.