This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS3.3能否运行在win8操作系统中?



大家好:

       1、请问 CCS3.3是否支持win8?如果支持,应该怎么安装,如果不支持,怎么解决。

       2、Seed-510Plus 是否支持 CCS5; 在64位 win7及win8系统中,Seed-510Plus能否使用。

谢谢

  • yulong

    win7都不支持。

    可以安装虚拟系统,然后把CCSv3.3装在虚拟xp中。我是用Oracle VM VirtualBox装的虚拟机。

     

    目前SEED-XDS510PLUS仿真器没有针对CCSV5的驱动,因此无法再CCSV5上使用。

    如果楼主使用SEED-XDS510PLUS仿真器,请用CCS4.1.3以下版本或者用CCS3.3。

    CCS4.13和CCS3.3都可以支持Piccolo的仿真。

    如果楼主在CCS4里面找不到相关型号,可以安装附件C2000芯片支持插件

    ti_c2000support_setup_2.1.0.2_ccsv4.rar

    Eric