关于芯片内M3核与C28核的位操作问题,如果使用C28核进行位操作与使用M3核进行位操作的不同;或者哪个核进行位操作时速度更快?M3核中可以通过“位带别名区”来实现对内存或是外设的某一位的操作,C28核是如何实现位操作的?谢谢各位了!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
关于芯片内M3核与C28核的位操作问题,如果使用C28核进行位操作与使用M3核进行位操作的不同;或者哪个核进行位操作时速度更快?M3核中可以通过“位带别名区”来实现对内存或是外设的某一位的操作,C28核是如何实现位操作的?谢谢各位了!
Eric,
还有个问题需要请教一下,关于M3核的位带别名区地址的问题。我如果对GPIO70这个管脚进行位操作,现在知道GPIOC的基址为0x40006000,GPIODATA的偏移地址为0x00,根据手册中的公式bit_word_addr = bit_band_base + (byte_offset x 32) + (bit_number × 4),bit_band_base为0x42000000,byte_offset为0x40006000,现在不知道bit_number的值应为多少?