我在编译CCSV4的时候有个问题,我是MSP430的积极用户,现在决定是用C2000。未来使用中需要小型化,但是我在编译代码时遇到困难。
我确实导入了名为controlSUITE的文件,像Wiki里说的那样,我创建了所有的目标新文件。但是当我编译的时候,显示如下的报错信息:
"Severity and Description Path Resource Location Creation Time Id
This project was created using a version of Code Generation tools that is not currently installed: 5.2.2 [C2000]. Please install the Code Generation tools of this version, or migrate the project to one of the supported versions. BlinkingLED properties 1315193267826 124 "
有谁能帮我一下吗?