有没有DSP28335使用CAN中断发送的例程?或者CAN发送中断怎么使用?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好,请问你的28335 eCAN收和发正常了吗。
我用eCAN A发和eCAN B 收,用SN65HVD235作的收发器,发现235的TX上有信号,但是量CANH和CANL上没有 波形,发送的TA一直置不了位,请问你遇到过这个问题吗?
今天上午终于把28335的CANA发CANB收搞定了,问题出在采购的SN65HVD235是假的,从TI官方申请的SN65HVD232和SN65HVD235都是可以正常收发的,但是从外面购买的235就是不行。
根据a to b例子,定义一个B接收邮箱,然后设定ABO为1,SUPS为1就可以收发了,折腾了好几天原来芯片是假的,很不爽。
TI官方的235除了顶层的丝印有外,在底部还有数字,而假的没有 。