This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我想通过SCI烧写程序,配置IO 口为SCI boot mode,GPIO18 为 3.3V,GPIO29为3.3V,GPIO34 为0.3V,
使用C2PROG V1.5 烧写程序,点击program ,目标板重新上电,显示如下所示:
CRC Info added at 0x003F6261: 0x6501 0xEF8C 0x0000
*** PLEASE RESET TARGET IN SCI BOOT-LOADER MODE ***
Connecting with target (autobaud)... failed (no response
过一会电流会增大,但GPIO18 电压会降至0.26V。
当在ccs下仿真调试时 SCI能和PC 机正常通信。
如果使用BOOT SCI 是否需要硬件设置或者其他项目需要设置?
非常感谢!
Hi Eric,
我已经将GPIO18 和GPIO29加上拉电阻,GPIO34加下拉电阻,当我按 program 烧写程序后 界面会显示failed(no response),
此时GPIO18的电平也被自动拉低,这是什么情况导致的呢?
谢谢!
donghui
donghui,
加下拉电阻一般1k, 2k都可以,但是你GPIO34加下拉电阻最好有个切换开关,因为当烧写完成后,需要将GPIO34切换成高电平,让芯片下次上电的时候能够引导到Flash中运行。
这块电路时没什么问题,但是不知道你的USB转串口这部分电路是如何设计的? 你写一个串口程序,以及PC端的串口助手,收发正常吗?
Eric
donghui,
你也可以参照下帖:
http://www.deyisupport.com/question_answer/microcontrollers/c2000/f/56/t/9864.aspx
Eric