Other Parts Discussed in Thread: TL431
前级PFC稳定母线电压,PFC输出的母线电压固有100Hz的两倍工频纹波,LLC的输出电压采用光耦+TL431进行闭环,发现此时LLC的输出电压上也有100Hz的纹波。
这个原因是光耦和431回路的响应速度太慢导致的吗?该怎么调节一下环路
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
前级PFC稳定母线电压,PFC输出的母线电压固有100Hz的两倍工频纹波,LLC的输出电压采用光耦+TL431进行闭环,发现此时LLC的输出电压上也有100Hz的纹波。
这个原因是光耦和431回路的响应速度太慢导致的吗?该怎么调节一下环路
我再TI官网找了一下使用光耦和TL431做闭环的电源,发现开关频率基本都是在100kHz的。我用光耦和TL431做闭环做了一个300kHz的电源,纹波总是达不到要求,想问您一下为什么光耦+TL431做闭环TI的参考设计都是100kHz的,是因为光耦和TL431不适合高频数字电源中吗?
没,就是想问一下高频下比如300kHz或者1MHz下LLC能否使用光耦+TL431进行闭环,会不会存在光耦的响应速度跟不上的问题。
因为我看TI的一下参考设计使用光耦和TL431进行闭环的一般系统的开关频率都是100kHz
高频下比如300kHz或者1MHz下LLC能否使用光耦+TL431进行闭环,会不会存在光耦的响应速度跟不上的问题。
TL431可与300kHz 至1MHz 的光耦合器配合使用,但是需要一个非常积极的补偿网络来最大限度地提高 TL431的带宽。 如果 TL431的带宽不足,使用分立式运算放大器和电压基准解决方案会更好。
是的,以下是一个100kHz 运算放大器设计 https://www.ti.com/tool/PMP21867
以及一个150kHz 运算放大器设计 https://www.ti.com/tool/PMP21943