This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

2812EV Timer1 and Timer2 联合使用T2CNT以及GPTCONA的问题



Hi TiSupport:

       我在测试GPTCONA的使用时,发现一个问题。

      1)T2PIN/T2PIN选择10时会有PWM波形输出,选择00时反而没有波形输出,好像和spec不相符。根据你们的经验是什么原因造成的?

      2)当我把T1和T2分别控制引脚输出时,没有问题,测试T2使用T1定时器控制时出现问题,我想问问

      2.1)T2CTRIPE/T1CTRIPE 以及 T2CMPOE/T1CMPOE设置是否应该同步,也就是说,同时为1或者同时为0。

      2.2)如果T2使用T1了,T2的TENABLE和TECMPR是否必须设置为0?