This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

28035的EPWM模块的TZ子模块问题



有2个配置说明不是很明白,请教TI高手。

在EPWM REFERENCE中关于TZ模块有2段话:

1、If the CBC interrupt is enabled via the TZEINT register, and DCAEVT2 or DCBEVT2 are selected as CBC trip sources via the TZSEL register, it is not necessary to also enable the DCAEVT2 or DCBEVT2 interrupts in the TZEINT register, as the DC events trigger interrupts through the CBC mechanism.

2、If the one-shot interrupt is enabled via the TZEINT register, and DCAEVT1 or DCBEVT1 are selected as OSHT trip sources via the TZSEL register, it is not necessary to also enable the DCAEVT1 or DCBEVT1 interrupts in the TZEINT register, as the DC events trigger interrupts through the OSHT mechanism.

我的理解:

第1条:DCAEVT2和DCBEVT2是工作在CBC机制下的,如果DCAEVT2和DCBEVT2被配置成TZ模块的CBC触发事件,那么不用在TZEINT中使能中断?

第2条:DCAEVT1和DCBEVT1是工作在OST机制下的,如果DCAEVT1和DCBEVT1被配置成TZ模块的OST触发事件,那么不用在TZEINT中使能中断?

是不是这样理解????

 

那么关于

DC模块的DCAEVT2和DCBEVT2工作在CBC机制下是怎么回事?

DCAEVT1和DCBEVT1是工作在OST机制又是怎么回事?

 

  • Lzh,

    关于DC模块,你对这两段话的理解是正确的,不过关于中断的一点,再确认一下,你可以查看TZEINT寄存器,里面包含对DC事件,CBC,OST事件的中断使能,这两段话的意思是,如果你将DC事件作为TZ模块的输入,由TZSEL寄存器配置,那么只要在TZEINT使能CBC或OST的中断就行了,不用使能DC事件中断。

    至于DC模块在CBC或OST下是怎么回事?你是想了解什么呢?

    比如DCAEVT2和DCBEVT2这两个事件可以配置为CBC的TZ输入,类似普通的TZ1,TZ2信号一样。同理DCAEVT1。

    至于怎么生成DC事件,则要看一下DC模块的解释。

    Eric

  • 你们这里的"DC模块"是指什么呢?DCBEVT1和DCBEVT2是不是可以这样认为,相当于可以用Comparator Output A或者Comparator Output B入口进行触发保护,来实现封锁pwm信号,其实和TZ触发是一样的,只是不同的GPIO输入口而已?