This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

调试flash api 问题



调试 api  2802x例子      编译 出现下面的警告:

Description    Resource    Path    Location    Type
#16002-D build attribute vendor section TI missing in "D:/dspworkspace_v5_2/flash_api/2802x/v201a/lib/Flash2802x_API_V201.lib<Flash28_ClearLoop.obj>": compatibility cannot be determined    test2             C/C++ Problem

仿真到: 

  Status = Flash_Erase((SECTORB|SECTORC|SECTORD),&FlashStatus);
   if(Status != STATUS_SUCCESS)
   {
       Example_Error(Status);
   }
  

出现如下问题:

Can't find a source file at "Flash28_Erase.c"
Locate the file or edit the source lookup path to include its location.