This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,
项目需求如下:采集信号传感器感应输出的模拟信号,该信号为瞬时脉冲信号,信号带宽10MHz,信号的采样时间<1s 数据采样率在2M左右,采样精度要求12b 。按1s 的采样时间算,则每次传感器有数据的时候数据量在4MB左右;
系统特点是采集信号为模拟量,采样率中等,是突发式瞬时触发采集而不是连续采集。
为提高系统集成度,不打算使用外部专用AD芯片,拟采用TMS320F2812,该芯片理论AD采样速度最高12.5MHz,想咨询下该芯片AD采集的精度,注意事项及采用校正算法时候的采样速度?
另为保证4MB的数据实时传输至PC机,有无成熟的数据传输方案推荐?
谢谢!!
1.、F2812的AD精度大概在9bit 左右,如果想提高精度建议使用F2833x或者F2823x。
2、F2812 TI官网有相关的AD Calibration的相关文档和历程。
3、此应用不是C2000的典型应用,因此无成熟的方案推荐。
4. 4MB/s的速度,建议使用SPI 或者 Mcbsp接口。