用的F28027。我在controlSUITE的example_f2802xCpuTimer基础上才增添几个小函数,就出现RAM溢出的error了,不至于啊??
error信息如下:
"C:/ti/controlSUITE/device_support/f2802x/v200/f2802x_examples/cpu_timer/../../F2802x_common/cmd/F2802x_generic_ram.cmd", line 112: error:
program will not fit into available memory. placement with
alignment/blocking fails for section ".cinit" size 0x1a page 0. Available
memory ranges:
RAMM0 size: 0x3b0 unused: 0x0 max hole: 0x0
RAML0 size: 0x400 unused: 0x18 max hole: 0x18
>> Compilation failure
.cinit : > RAMM0 | RAML0, PAGE = 0
error: errors encountered during linking; "Example_F2802xCpuTimer.out" not
built