This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

2407A中断嵌套



2407A是否可以实现中断嵌套?嵌套逻辑是什么样的?低优先级中断能打入高优先级中断么?如果仅想实现高优先级中断打入低优先级中断,需要做哪些处理?谢谢!

  • C2000都可以实现中断嵌套,但默认是不使能的。低优先级不能打断高优先级。

    LF2407A是非常老的片子,如果是做新的设计,建议使用Piccolo系列,性价比高。

  • 请问怎样使能呢?进入ISR后先进行enable么?书中推荐的方式是在每个ISR最后enable。我做个了测试程序,貌似在默认ISR结构下,INT0可以嵌入INT1,INT1也可以嵌入INT0,总觉得怪怪的,但进行代码跟踪的时候确实发现了这样的情况,如何避免INT1嵌入INT0呢?

  • 首先,以TI提供的英文原版的user guide或technical manual为准,其它的书籍也好,文档也好,特别是翻译的,只用来辅助你理解。

    其次,不建议你使用LF240x的东西,即便是F281x的也不推荐,除了价格供货等方面的原因,技术支持后面也会跟不上的。