This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

串口SCI下载程序 boot



我已经将DSP管脚设置成SCI下载程序模式,将PC机与DSP通过串口连接,利用串口助手发送AA08控制指令,DSP能返回AA0的值,之后就直接跳到DSP之前下载的主程序里了,请问是为什么呢?

  • 您好,yafang

     

    建议您先从以下几个方面尝试解决:

    (1)您通过何种串口方式连接PC机与C2000?

    (2)您使用的串口通讯速率是多少?(C2000能够在boot load的过程中识别并同步通讯速率,但是建议您使用较为常用的通讯速率)

    (3)请问您在发送完AA08控制指令后,是否有尝试继续后面的数据流操作?

     

    另外,请问您使用的芯片Part Number是哪一颗?是否每次操作都会有同样的结果?