资料里写的F28系列的最高采样带宽为12.5MSPS。 但实际用epwm定时器触发AD采样到1.6M时就已经不稳了。 请问这个采样12.5M是如何实现的。
谢谢!!!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
资料里写的F28系列的最高采样带宽为12.5MSPS。 但实际用epwm定时器触发AD采样到1.6M时就已经不稳了。 请问这个采样12.5M是如何实现的。
谢谢!!!
例程里的没有那么高的采样率。
我指的“不稳”,是指每次采样的间隔有误差。比如用epwm定时出发AD,在AD中断程序中写入“ GpioDataRegs.GPATOGGLE.bit.GPIO21 ”, 然后用示波器观察GPIO21跳变的状态,发现上没冲宽度宽窄有偏差,不匀。 我们做的采样频率是2M, 比较快,对于采样频率要求也比较高。因此想问一下,文档里写的12.5M采样频率这个指标是如何测定的,也希望TI的工程师能给与我们一些建议,谢谢您!!!
请查看数据手册6.10.7.3 Sequential Sampling Mode (Single-Channel) (SMODE = 0)和ADC用户手册Figure 1-9. ADC Core Clock and Sample-and-Hold (S/H) Clock,这个频率指的是S/H clock pulse,也即采样保持所花的时间,而不是两个采样之间的时间。
需要区别采样间隔和采样频率,前者是指两个采样之间的时间,而后者是指采样一个信号所需要的时间。