This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

F28069调试问题

Other Parts Discussed in Thread: MOTORWARE

大家好,请教一下,我用controlstick小板子在调试motorware中的例程时出现有15个错误,无法load程序

第一个是

Description Resource Path Location Type <a href="file:/F:/New%20Folder/ccsv5/tools/compiler/dmed/HTML/16008.html">#16008-D</a>  file proj_lab05d    C/C++ Problem

第二个是

Description Resource Path Location Type #99900 error limit reached; 100 errors detected proj_lab05d    C/C++ Problem

其他几个在f28069M_ram_lnk.cmd文件中

MEMORY { PAGE 0 :

   BEGIN       : origin = 0x000000, length = 0x000002    /* BEGIN is used for the "boot to SARAM" bootloader mode   */    RAMM0       : origin = 0x000050, length = 0x0003B0    RAML0_L3    : origin = 0x008000, length = 0x002000  /* on-chip RAM block RAML0-L3 */

   RESET       : origin = 0x3FFFC0, length = 0x000002    FPUTABLES   : origin = 0x3FD590, length = 0x0006A0  /* FPU Tables in Boot ROM */    IQTABLES    : origin = 0x3FDC30, length = 0x000B50    /* IQ Math Tables in Boot ROM */    IQTABLES2   : origin = 0x3FE780, length = 0x00008C    /* IQ Math Tables in Boot ROM */    IQTABLES3   : origin = 0x3FE80C, length = 0x0000AA  /* IQ Math Tables in Boot ROM */

   BOOTROM    : origin = 0x3FF3B0, length = 0x000C10

PAGE 1 :

   BOOT_RSVD   : origin = 0x000002, length = 0x00004E    /* Part of M0, BOOT rom will use this for stack */    RAMM1       : origin = 0x000400, length = 0x000400    /* on-chip RAM block M1 */    RAML4_6     : origin = 0x00A000, length = 0x006000    /* on-chip RAM block L4 to L6 */    USB_RAM     : origin = 0x040000, length = 0x000800    /* USB RAM */ }

(这是复制文件中的部分,在 length =0x后面换行)

console中显示

C28xx: GEL: Encountered a problem loading file: E:\ti\motorware\motorware_1_01_00_07\sw\solutions\instaspin_motion\boards\hvkit_rev1p1\f28x\f2806xM\projects\ccs5\proj_lab05d\Debug\proj_lab05d.out Could not open file