This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
拿到一套DRV8312-69M-KIT 三相电机控制套件:50V、3.5A Piccolo F28069M、InstaSPIN™-FOC。
我的controlSuite版本是v3.0.3,在里面找不到这个套件里的F2806x ISO controlCARD RELEASE 0.2的电路文件, 是我的版本太低吗,还是要到别的地方找?
我的motorware版本是1.01.00.05,里面有10个28069m InstaSPIN-FOC的示例程序,我不知道哪个是这个套件的代码,麻烦能告诉下吗?
另外,我用的CCS版本是5.2.1.00018,怎么用快捷键加书签和查找书签?我在window下拉菜单的Preferences/General/Keys里加了快捷键但不好用啊?应该怎么弄?麻烦告诉下,谢谢啦。
您好,Xin Gao
(1)请问您要找的是不是F2806XISO-CONTROLCARDR0.3-SCH?
(2)...\motorware\motorware_1_01_00_08\sw\solutions\instaspin_motion\boards\drv8312kit_revD\f28x\f2806xM\projects\ccs5
这个目录下的应该都是这个套件的示例工程。
(3)关于操作书签的快捷键我没有找到,希望您找到之后能够与大家分享,谢谢
Motorware有新的版本1.01.00.08,里面的lab程序都是分为FOC和Motion的,每个lab程序实现的目的和框图等在User's Guide中都有。软件和手册在
www.ti.com/motorware 中下载。谢谢!
Hui,
套件可以直接在 TI Store上购买,支持支付宝的;不需要其他附件了,套件里面自带功率部分和controlcard;套件功能比较强大,但注意供电和带的负载大小,8312是低压低电流套件。