This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

28335的晶振问题



       我在画板时发现28335的外部有源晶振在接25MHZ时一切正常连接仿真口,但是在连接30Mhz有源晶振(3.3V)并连接仿真器时就出现了假死状态。DSP连接不上且各个IO口状态也是异常,外部上拉却输出低电平。

      并且最奇怪的是28232和335是同系列晶振部分推荐无源晶振是20~35Mhz,有源4~100/150M,但是发现有用无源10M晶振也能正常工作的且一大批量使用,对此很疑惑????

      因此问下各位大神是否TI 28系列外部晶振对芯片有什么影响是否有相应文档????

  • 1. 10M可以使用是TI不保证的,也即有可能会出问题的情况,所以建议更改到规格书要求的范围;

    2. 不知道你的晶振电路是怎么设计的?我猜想可能跟这有关系;

    3. 文档没有特别专门讲晶振的,但可以参考的是数据手册里你看过的规格以及3.6 System Control部分,另外还有一本硬件设计指南可对照一下 Hardware Design Guidelines for TMS320F28xx and TMS320F28xxx DSCs (Rev. A),序列号:spraas1,版本B.