This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于基于28027launchpad的LCD问题

Other Parts Discussed in Thread: CONTROLSUITE

请问TI的老师,我用12864液晶显示一下字符,能够烧进去,可是为什么12864不显示?这个程序是串行输入数据让LCD显示电气工程学院,电气工程与自动化,张大山,11112222,用LCD的CLK,SID,CS接GPIO7,6,5,使用其通用IO功能,用程序模拟CLK时钟。

#include "DSP28x_Project.h" // Device Headerfile and Examples Include File


char table0[]="电气工程学院";
char table1[]="电气工程与自动化";
char table2[]="张大山";
char table3[]="11112222";

//******************delay*************************//
void delay_ms (Uint16 ms)
{
Uint16 i,j;
for(i=0;i<ms;i++) //外层循环若干毫秒
{
for(j=0;j<6000;j++); //内层循环1毫秒定时
}
}

//******************GPIO configure****************//
void Gpio_Init(void)
{
EALLOW;
GpioCtrlRegs.GPAMUX1.all = 0x00000000; // All GPIO//MUX寄存器是多路复用寄存器,低电平代表不复用,使用的时候要进行保护
GpioCtrlRegs.GPAMUX2.all = 0x00000000; // All GPIO
GpioCtrlRegs.GPBMUX1.all = 0x00000000; // All GPIO
GpioCtrlRegs.GPADIR.all = 0xFFFFFFFF; // All outputs
GpioCtrlRegs.GPBDIR.all = 0x0000000F; // All outputs
EDIS;
}
//******************Datas sending function*************//
void Sendbyte(unsigned char data1)//发送指令或数据的函数
{
unsigned int i;
for(i=0;i<8;i++)
{
GpioDataRegs.GPADAT.bit.GPIO7=0; //GPIO0 is CLK
if(data1&0x80)
GpioDataRegs.GPADAT.bit.GPIO6=1; //GPIO1 is data output pin
else
GpioDataRegs.GPADAT.bit.GPIO6=0;
GpioDataRegs.GPADAT.bit.GPIO7=1;
data1=data1<<1;
delay_ms(1);
}
}

//******************Command sending function*************//
void write_com(unsigned char com)
{
GpioDataRegs.GPADAT.bit.GPIO5=1;//串行使能
Sendbyte(0xf8);//表示接下来要发送命令
Sendbyte(com&0xf0);//表示发送第二个字节的高4位
Sendbyte((com&0x0f)<<4);//表示发送第3个字节的低4位
GpioDataRegs.GPADAT.bit.GPIO5=0;//串行使能
delay_ms(1);
}

//******************Display data sending function*************//
void write_data(unsigned char data)
{
GpioDataRegs.GPADAT.bit.GPIO5=1;//串行使能
Sendbyte(0xfa); //表示接下来要发送数据 //That is to say
Sendbyte(data&0xf0);//表示发送第二个字节的高4位
Sendbyte((data&0x0f)<<4);//表示发送第3个字节的低4位
GpioDataRegs.GPADAT.bit.GPIO5=0;//串行使能
delay_ms(1);
}
void LCD_Init()
{
write_com(0x01);//清楚LCD显示内容
write_com(0x30);//8位数据
write_com(0x0c);//显示开,关光标
write_com(0x06);//游标及显示右移一位
write_com(0x02);//清DDRAM
}

void main(void)
{
unsigned int n;

InitSysCtrl();


Gpio_Init();


DINT; //屏蔽中断


InitPieCtrl(); //初始化中断控制寄存器


IER = 0x0000; //中断使能寄存器,某一位是1表示使能中断
IFR = 0x0000; //中断标志寄存器,某一位是1表示产生中断标志


InitPieVectTable();//初始化中断向量表,把向量表复制到指定RAM段,防止非法中断的产生


LCD_Init();

//************************The first line**********************//
write_com(0x80);//第一行
write_data(0x0b);
write_data(0x0b);
for(n=0;n<12;n++)
{
write_data(table0[n]);
delay_ms(1);
}
write_data(0x0b);
write_data(0x0b);


//************************The second line**********************//
write_com(0x90);
for(n=0;n<16;n++)
{
write_data(table1[n]);
delay_ms(1);
}


//************************The third line**********************//
write_com(0x88);
write_data(0x03);
write_data(0x03);
for(n=0;n<6;n++)
{
write_data(table2[n]);
delay_ms(1);
}
write_data(0x03);
write_data(0x03);


//************************The fourth line**********************//
write_com(0x98);
for(n=0;n<8;n++)
{
write_data(table3[n]);
delay_ms(1);
}

while(1);
}