This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
现用28069内部比较器做过流保护,产生DCAEVT1和DCBEVT1事件,同时,又把这个内部比较器的值输出到芯片外部再回到芯片的TZ1引脚,产生OSHT1事件,将ePWM配制成响应DCAEVT1、DCBEVT1和OSHT1事件,现在如果产生过流,在TZFLG寄存器了,是不是DCAEVT1、DCBEVT1和OST会被同时置位呢?
DC本身就是ePWM模块的一个子模块,可以通过one-shot模式触发ePWM的动作,也可以产生中断,为什么还要将它输出至一个GPIO口重新输入并设置呢?
建议再仔细看下TRM,高效地利用这个模块。