您好!我想问您几个问题,以便从宏观上把握系统移植这个概念。
1、针对F28m35这个双核的芯片,我们是要建立两个project。那么我们如果要做一个TI-RTOS的移植,这个工程是属于哪个工程?是C28X的,还是M3的?
2、我在CCS中打开了下载的TI-RTOS,里面有很多的demo和example,每个工程的例子里面有很多的文件。如果要添加自己的一些功能,需要修改哪些文件?
谢谢指导!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好!我想问您几个问题,以便从宏观上把握系统移植这个概念。
1、针对F28m35这个双核的芯片,我们是要建立两个project。那么我们如果要做一个TI-RTOS的移植,这个工程是属于哪个工程?是C28X的,还是M3的?
2、我在CCS中打开了下载的TI-RTOS,里面有很多的demo和example,每个工程的例子里面有很多的文件。如果要添加自己的一些功能,需要修改哪些文件?
谢谢指导!
您好!
TI-RTOS示例代码中好像没有配置管脚的代码,可以参考以下方式对分配给C28核的IO口进行设置,其中的GPIO_PORTX_BASE及0xNN值请根据需要并参考使用手册进行设置, GPIO_PIN_C_CORE_SELECT表示端口分配给c28核。不做以下处理的GPIO口,默认分配给m3侧使用。
GPIOPinConfigureCoreSelect(GPIO_PORTX_BASE, 0xNN, GPIO_PIN_C_CORE_SELECT);
谢谢!