This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

InitPieVectTable疑惑



在DSP2833x_PieVect.c中

void InitPieVectTable(void)

{

   int16   i;

   Uint32 *Source = (void *) &PieVectTableInit;

   Uint32 *Dest = (void *) &PieVectTable;

   EALLOW;      

   for(i=0; i < 128; i++)

   *Dest++ = *Source++;      

   EDIS;

   // Enable the PIE Vector Table

   PieCtrl.PIECRTL.bit.ENPIE = 1;        

}

Uint32 *Source = (void *)&PieVectTableInit

此句的强制指针转换,在单独的VC编译下显示是错误的:

error: invalid conversion from `void*' to `int*'

为什么在这个地方可以正确使用?