This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
看了比较多的关于F2812的资料后,终于想动手一下,于是写了看上去超简单的一个程序,其实也真的很简单。
asm文件:
.GLOBAL _c_int00
.text
_c_int00:
ADD ACC,#1
.end
cmd文件:
MEMORY
{
PAGE 0 : PROG : origin=0x3f8000,length=0x1fff
}
SECTIONS
{
.text : >PROG,PAGE=0
}
编译->load program->run
出现以下错误:
Trouble running Target CPU: Can't write to data MEMORY 0x801, check MEMORY config [-2184]
ACC是加1了,在按run,出现以下错误:
Can't Run Target CPU: Can't write to data MEMORY 0x803, check MEMORY config [-2184]
这次ACC没有加1,再按run也没有其他反应了(地址加2->0x805,以此类推)
我看了,0x800-0xD00是不可以随便用的,但我好像没有招惹它,为什么会有这样的问题?请高手指点迷路
您好!
首先不要轻易改写Code Start Branch 文件。
您要做的任务是在TI的头文件等基础上改写。
关于你的问题:
Begin Section是 0x3F8000, 而且必须是2个word。
因为CodeStart里面放了一个长跳转指令LB,刚好是2个word。
.sect "codestart"
code_start:
.if WD_DISABLE == 1
LB wd_disable ;Branch to watchdog disable code
.else
LB _c_int00 ;Branch to start of boot.asm in RTS library
.endif
SECTIONS
{
/* Setup for "boot to H0" mode:
The codestart section (found in DSP28_CodeStartBranch.asm)
re-directs execution to the start of user code.
Place this section at the start of H0 */
codestart : > BEGIN, PAGE = 0
.
.
.
}