This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Piccolo28035 ADC转换最大可承受多大电压值?
F2802x/3x系列的ADC模块支持满量程的模拟信号输入即0~3.3V,AD端口能够承受的电大电压(保证芯片不被损坏)是另外一个参数,称做绝对最大允许范围 -0.3~4.6V (对Vdd,Vddio和GPIO也同样适用),所以任何引脚的信号输入都不能超出这个范围. 当使用3.3V作为ADC的参考电压时,超过3.3V但小于4.6V的电压将被处理成12位对应的最大数字转换结果4095,若ADC模块使用外部电源做参考,则超过Vrefh而小于4.6V的电压对应的结果都是4095.
谢谢你我以前以为只能接小于3.3不能大于一点点呢, 原来耐压我我想象的大! 不知道一直大于3.3V小于4.6V会怎样?
芯片的工作电压是3.3V,但都是有一个范围的,比如Piccolo系列的是+/-10%,另外一个就是上面提到的绝对最大值。
当你的输入电压在3.3~3.63V之间时,芯片是可以正常工作的,但在3.63~4.6V之间则不能保证,有可能继续采样继续工作,也有可能出现异常。具体参数请参考数据手册第6章前两节。