Part Number: TMS320F28377S
你好,需要使用两台DSP的ePWM的载波同步功能。现在有两个问题:1:SYNCI信号是否可以配置为任意GPIO引脚。2:这个同步信号的产生机理是什么,波形是什么样子的。3:两台DSP采用竞争机制,即谁先启动,谁做主机,来发SYNC同步信号,这种使用模式下,Input X-bar和output X-bar如何配置。谢谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TMS320F28377S
你好,需要使用两台DSP的ePWM的载波同步功能。现在有两个问题:1:SYNCI信号是否可以配置为任意GPIO引脚。2:这个同步信号的产生机理是什么,波形是什么样子的。3:两台DSP采用竞争机制,即谁先启动,谁做主机,来发SYNC同步信号,这种使用模式下,Input X-bar和output X-bar如何配置。谢谢
1、是的,如原帖所述,通过Input X-bar可以将任意GPIO配置为SYNCI。
2、同步信号其实就是一个脉冲信号/时钟信号,也就是方波。产生机理。。。这个得看你是用的什么来源的同步信号,可以外部引入,也可以由PWM模块本身产生。
3、这点说实话没这方面的案例,不确定能否实现。个人想法是做一个逻辑判断,基于这个判断设计两个执行语句来对Input/Output X-bar和同步寄存器进行配置。