Part Number: TMS320F28388D
Other Parts Discussed in Thread: SFRA,
SFRA run in CPU2 can't sweep well in SFRA GUI.
I try to run SFRA In TMS320F28388D both cpu. In CPU01, it work fine, can both communication and sweep. However, In CPU02, it can communication but get stuck at sweep(when i click "start sweep" at GUI, it always stuck, GUI become gray and can't see any change in progress bar. but when debug it, the "freqindex" already achieve to 22 which is the "veclength" ).Just like below:

Below in my configure, i do the same in cpu01, and it work fine.
in flash cmd files:

The lib and path i use in cpu02


when i run sfra in cpu02, i have mask the sfra in cpu01.
How can i fix this, does anyone can provide some help?