Part Number: TMS320F280025
Other Parts Discussed in Thread: C2000WARE
已经通过lin口把bin文件烧写入flash了,但是不知道一些配置如何配置,导致最后跳转到主程序main的时候进入Interrupt_illegalOperationHandler错误中断,请教下
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TMS320F280025
Other Parts Discussed in Thread: C2000WARE
已经通过lin口把bin文件烧写入flash了,但是不知道一些配置如何配置,导致最后跳转到主程序main的时候进入Interrupt_illegalOperationHandler错误中断,请教下
额,抱歉直接把工程发上来的话其实像我们对工程不了解的诊断起来会有的吃力啊。
你的项目应该是要实现二次boot,不过用lin的方式boot我这边没有这方面的实操经验,但是TI是有提供一个基于SCI的二次bootloader例程的,你可以参考例程里面的跳转方法和跳转地址:
C:\ti\c2000\C2000Ware_4_01_00_00\driverlib\f28002x\examples\flash
-stack 0x380
MEMORY
{
BEGIN : origin = 0x080000, length = 0x000002
BOOT_RSVD : origin = 0x00000002, length = 0x00000126
RAMM0 : origin = 0x00000128, length = 0x000002D8
RAMM1 : origin = 0x00000400, length = 0x000003F8 /* on-chip RAM block M1 */
// RAMM1_RSVD : origin = 0x000007F8, length = 0x00000008 /* Reserve and do not use for code as per the errata advisory "Memory: Prefetching Beyond Valid Memory" */
/* RAMLS4 : origin = 0x0000A000, length = 0x00000800
RAMLS5 : origin = 0x0000A800, length = 0x00000800
RAMLS6 : origin = 0x0000B000, length = 0x00000800
RAMLS7 : origin = 0x0000B800, length = 0x00000800*/
/* Combining all the LS RAMs */
RAMLS4567 : origin = 0x0000A000, length = 0x00002000
RAMGS0 : origin = 0x0000C000, length = 0x000007F8
// RAMGS0_RSVD : origin = 0x0000C7F8, length = 0x00000008 /* Reserve and do not use for code as per the errata advisory "Memory: Prefetching Beyond Valid Memory" */
BOOTROM : origin = 0x003F0000, length = 0x00008000
BOOTROM_EXT : origin = 0x003F8000, length = 0x00007FC0
RESET : origin = 0x003FFFC0, length = 0x00000002
/* Flash sectors */
/* BANK 0 */
FLASH_BANK0_SEC0 : origin = 0x080002, length = 0x001FFE /* on-chip Flash */
FLASH_BANK0_SEC1 : origin = 0x082002, length = 0x00cffe /* on-chip Flash */
/*
FLASH_BANK0_SEC2 : origin = 0x082000, length = 0x001000
FLASH_BANK0_SEC3 : origin = 0x083000, length = 0x001000
FLASH_BANK0_SEC4 : origin = 0x084000, length = 0x001000
FLASH_BANK0_SEC5 : origin = 0x085000, length = 0x001000
FLASH_BANK0_SEC6 : origin = 0x086000, length = 0x001000
FLASH_BANK0_SEC7 : origin = 0x087000, length = 0x001000
FLASH_BANK0_SEC8 : origin = 0x088000, length = 0x001000
FLASH_BANK0_SEC9 : origin = 0x089000, length = 0x001000
FLASH_BANK0_SEC10 : origin = 0x08A000, length = 0x001000
FLASH_BANK0_SEC11 : origin = 0x08B000, length = 0x001000
FLASH_BANK0_SEC12 : origin = 0x08C000, length = 0x001000
FLASH_BANK0_SEC13 : origin = 0x08D000, length = 0x001000
FLASH_BANK0_SEC14 : origin = 0x08E000, length = 0x001000
*/
FLASH_BANK0_SEC15 : origin = 0x08F000, length = 0x000FF0
// FLASH_BANK0_SEC15_RSVD : origin = 0x08FFF0, length = 0x000010 /* Reserve and do not use for code as per the errata advisory "Memory: Prefetching Beyond Valid Memory" */
}
SECTIONS
{
codestart : > BEGIN, ALIGN(8)
.text : >> FLASH_BANK0_SEC0, ALIGN(8)
.cinit : > FLASH_BANK0_SEC0, ALIGN(8)
.switch : > FLASH_BANK0_SEC0, ALIGN(8)
.reset : > RESET, TYPE = DSECT /* not used, */
.stack : > RAMM1
.init_array : > FLASH_BANK0_SEC0, ALIGN(8)
.bss : > RAMLS4567
.bss:output : > RAMLS4567
.bss:cio : > RAMGS0
.const : > FLASH_BANK0_SEC0, ALIGN(8)
.data : > RAMLS4567
.sysmem : > RAMLS4567
ramgs0 : > RAMGS0
GROUP
{
.TI.ramfunc
{ -l FlashAPI_F28002x_FPU32.lib}
}LOAD = FLASH_BANK0_SEC0,
RUN = RAMLS4567,
LOAD_START(RamfuncsLoadStart),
LOAD_SIZE(RamfuncsLoadSize),
LOAD_END(RamfuncsLoadEnd),
RUN_START(RamfuncsRunStart),
RUN_SIZE(RamfuncsRunSize),
RUN_END(RamfuncsRunEnd),
ALIGN(8)
DataBufferSection : > RAMGS0, ALIGN(8)
}
/*
//===========================================================================
// End of file.
//===========================================================================
*/
/*
//===========================================================================
// End of file.
//===========================================================================
*/
-stack 0x380
MEMORY
{
BEGIN : origin = 0x082000, length = 0x000002
BOOT_RSVD : origin = 0x00000002, length = 0x00000126
RAMM0 : origin = 0x00000128, length = 0x000002D8
RAMM1 : origin = 0x00000400, length = 0x000003F8 /* on-chip RAM block M1 */
// RAMM1_RSVD : origin = 0x000007F8, length = 0x00000008 /* Reserve and do not use for code as per the errata advisory "Memory: Prefetching Beyond Valid Memory" */
/* RAMLS4 : origin = 0x0000A000, length = 0x00000800
RAMLS5 : origin = 0x0000A800, length = 0x00000800
RAMLS6 : origin = 0x0000B000, length = 0x00000800
RAMLS7 : origin = 0x0000B800, length = 0x00000800*/
/* Combining all the LS RAMs */
RAMLS4567 : origin = 0x0000A000, length = 0x00002000
RAMGS0 : origin = 0x0000C000, length = 0x000007F8
// RAMGS0_RSVD : origin = 0x0000C7F8, length = 0x00000008 /* Reserve and do not use for code as per the errata advisory "Memory: Prefetching Beyond Valid Memory" */
BOOTROM : origin = 0x003F0000, length = 0x00008000
BOOTROM_EXT : origin = 0x003F8000, length = 0x00007FC0
RESET : origin = 0x003FFFC0, length = 0x00000002
/* Flash sectors */
/* BANK 0 */
FLASH_BANK0_SEC0 : origin = 0x080002, length = 0x001FFE /* on-chip Flash */
FLASH_BANK0_SEC1 : origin = 0x082002, length = 0x00CFFE /* on-chip Flash */
/*
FLASH_BANK0_SEC2 : origin = 0x082000, length = 0x001000
FLASH_BANK0_SEC3 : origin = 0x083000, length = 0x001000
FLASH_BANK0_SEC4 : origin = 0x084000, length = 0x001000
FLASH_BANK0_SEC5 : origin = 0x085000, length = 0x001000
FLASH_BANK0_SEC6 : origin = 0x086000, length = 0x001000
FLASH_BANK0_SEC7 : origin = 0x087000, length = 0x001000
FLASH_BANK0_SEC8 : origin = 0x088000, length = 0x001000
FLASH_BANK0_SEC9 : origin = 0x089000, length = 0x001000
FLASH_BANK0_SEC10 : origin = 0x08A000, length = 0x001000
FLASH_BANK0_SEC11 : origin = 0x08B000, length = 0x001000
FLASH_BANK0_SEC12 : origin = 0x08C000, length = 0x001000
FLASH_BANK0_SEC13 : origin = 0x08D000, length = 0x001000
FLASH_BANK0_SEC14 : origin = 0x08E000, length = 0x001000
*/
FLASH_BANK0_SEC15 : origin = 0x08F000, length = 0x000FF0
// FLASH_BANK0_SEC15_RSVD : origin = 0x08FFF0, length = 0x000010 /* Reserve and do not use for code as per the errata advisory "Memory: Prefetching Beyond Valid Memory" */
}
SECTIONS
{
codestart : > BEGIN, ALIGN(8)
.text : >> FLASH_BANK0_SEC1, ALIGN(8)
.cinit : > FLASH_BANK0_SEC1, ALIGN(8)
.switch : > FLASH_BANK0_SEC1, ALIGN(8)
.reset : > RESET, TYPE = DSECT /* not used, */
.stack : > RAMM1
.init_array : > FLASH_BANK0_SEC1, ALIGN(8)
.bss : > RAMLS4567
.bss:output : > RAMLS4567
.bss:cio : > RAMGS0
.const : > FLASH_BANK0_SEC1, ALIGN(8)
.data : > RAMLS4567
.sysmem : > RAMLS4567
ramgs0 : > RAMGS0
GROUP
{
.TI.ramfunc
{ -l FlashAPI_F28002x_FPU32.lib}
}LOAD = FLASH_BANK0_SEC1,
RUN = RAMLS4567,
LOAD_START(RamfuncsLoadStart),
LOAD_SIZE(RamfuncsLoadSize),
LOAD_END(RamfuncsLoadEnd),
RUN_START(RamfuncsRunStart),
RUN_SIZE(RamfuncsRunSize),
RUN_END(RamfuncsRunEnd),
ALIGN(8)
DataBufferSection : > RAMGS0, ALIGN(8)
}
/*
//===========================================================================
// End of file.
//===========================================================================
*/
/*
//===========================================================================
// End of file.
//===========================================================================
*/
请问下这两个cmd的地址这样配置,为什么跳转0x82000的时候总是进入Interrupt_illegalOperationHandler错误中断啊