This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
背景:CCS软件为12.0版本、C2000Ware_4_01_00_00、新买的TMS320F28388D开发板和XDS110仿真器
问题:根据开发板手册完成接线后,通过CCS打开例程进行测试仿真器是否接上时,出现错误。
另外在仿真器连接测试期间XDS110的D2灯亮红色并闪烁
希望能告知解决方法和查找问题的测试方法,谢谢!
连接报错信息:
The explanation is:
The JTAG IR and DR scan-paths cannot circulate bits, they may be broken.
An attempt to scan the JTAG scan-path has failed.
The target's JTAG scan-path appears to be broken
with a stuck-at-ones or stuck-at-zero fault.
Debug报错
Error connecting to the target: (Error -2131 @ 0x0)
Unable to access device register. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK).
(Emulation package 9.8.0.00235)
连接测试和Debug报错图片:
接线实物图片:
你好,因为你的图片有挡住一个接口,我不知道你是具体怎么连接的。
但是从图上来看,你不仅外接了XDS110仿真器,controlCARD上的板载仿真器你也连接了。
底板(TMDSHSECDOCK)上的J17和J1是电源口,J2是仿真器接口。
controlCARD上的J1:A是仿真器接口,J3是电源口。
你可以选择两块板子上的任一电源口+任一仿真器接口进行连接应该就可以了。
你好,我看到你的controlCARD上似乎没有LED灯是亮的?
或者你试一下直接用controlCARD上的电源和仿真器吧,也就是只用USB线连接J1:A和J3。
是的,D2:A是仿真器灯,D5是电源灯。另外J1:A接口只要找根对应的USB线就行了,这个口就是数据线口,仿真器是板载的XDS100 V2仿真器。
按照上述连接之后仿真器能正常连接烧写了吗?
另外,我不知道你的target configuration里面对XDS110有没有做设置修改?