This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
发送字符和16位数据原理是相同的。
一般情况下发送一个字符的格式为1位起始位+8位数据位(字符ASCII码)+1位结束位,从8位数据发送缓冲寄存器中取出数据进行发送。具体过程为:
在FIFO使能的情况下,首先发送数据缓冲寄存器SCITXBUF从TX FIFO中获取由CPU加载的需要发送的数据,然后SCITXBUF将数据传输发送给移位寄存器TXSHT,如果发送使能,TXSHT将接收到的数据逐位移到SCITXD引脚上
非常感谢你的回答,不过我想问的是dsp中16位数据怎么通过SCI的8位发送缓冲器发送,例如 SciaRegs.SCITXBUF=S 这条语句,如果S是一个字符变量,在dsp中占16位,那么发送的时候是截取低8位还是分两次发送 还是别的方式??