This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我是一个新手。我买了TI的HVMotorCtrl+PfcKit开发套件。连接了USB口,外置15V电源,SW1置于ON位置,插上了Piccolo F2803X controlCARD,在连接目标板时出现提示“Error connecting to the target:
Error 0x80000240/-151
Fatal Error during: Initialization, OCS, ”,是什么原因?前几天还是可以连上的,什么都没动,怎么连不上了?
建议参照操作手册,重新操作一次。
另外,请查看一下 USB接口是否正常,能否找到XDS100仿真器。
今天又能连上了,却编译不能通过了。提示的内容是“This project was created using a version of Code Generation tools that is not currently installed :5.2.3[c2000].Please install the Code Generation tools of this version, or mogration the project to one of the supported versions.”。我升级CCS4,升级ControlSUITED都无济于事。
今天又能连上了,却编译不能通过了。提示的内容是“This project was created using a version of Code Generation tools that is not currently installed :5.2.3[c2000].Please install the Code Generation tools of this version, or mogration the project to one of the supported versions.”。我升级CCS4,升级ControlSUITED都无济于事。
您好!
CCS4
Help->Software Updates 去更新CGT。
谢谢您!我不知更新了多少次了!我在D:\Program Files\Texas Instruments\ccsv4\tools\compiler\c2000目录的README.txt文档中看到版本是6.0.1的。怎么在错误提示中说是“5.2.3”?
我用的是HVMotorCtrl+PfcKit开发套件,里面应该是XDS100,设备管理器里面却显示Texas Instruments XDS560 PCI JTAG Emulator ,旁边有个"!"号,说明设备还不能正常工作.但HVMotorCtrl+PfcKit的LD1灯是亮了.但现在CCS4又不能编译了,所以也不知道有没有连上.
各位热心的专家,再次感谢你们的帮助!
今早我终于找到了问题的所在:Project/properties/CCS Build中的Code Generation tools选项卡中有"TI V5.2.3"和"TI V6.0.1"两个可选,我选了后者,问题立刻解决!
不过我还有很基础的问题要问,希望大家继续帮我.
非常感谢各位专家的帮助.
早上发现Project/properties/CCS Build的Code Generation tools选项卡中有"TI V5.2.3"和"TI V6.0.1"可选,选了后者问题立刻解决!