This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F280039C: TMS320F280039的GPIO18如何配置为CAN RX功能

Part Number: TMS320F280039C


您好!

      目前我们的板子GPIO19,X1是连接了外部晶振,代码中InitSysCtrl()里面配置是InitSysPll(XTAL_OSC, IMULT_48, REFDIV_2, ODIV_4, PLLCLK_BY_1, SYSCTL_DCC_BASE0),然后想把GPIO18配置为CAN RX功能,但是目前测试CAN收发一直没有通信上,请问GPIO18这可以这样子应用吗?

      因为我在其他帖子里看了比如280049的GPIO18配置为其他功能好像是需要配置为使用内部晶振且X1下拉,我不确定280039的GPIO18配置为CAN RX是不是也要这样做。