This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

28027launchpad SPI问题



请看我这段程序,为什么用示波器观察SPICLKA即18脚观察不到方波?

//#############################################################################
//
// File: f2802x_examples_ccsv4/spi_loopback/Example_F2802xSpi_FFDLB.c
//
// Title: F2802x Device Spi Digital Loop Back program.
//
// Group: C2000
// Target Device: TMS320F2802x
//
//! \addtogroup example_list
//! <h1>SPI Digital Loop Back</h1>
//!
//! This program is a SPI example that uses the internal loopback of
//! the peripheral. Interrupts are not used.
//!
//! A stream of data is sent and then compared to the recieved stream.
//!
//! The sent data looks like this:
//! 0000 0001 0002 0003 0004 0005 0006 0007 .... FFFE FFFF
//!
//! This pattern is repeated forever.
//!
//! Watch Variables:
//! - sdata - sent data
//! - rdata - received data
//
// (C) Copyright 2012, Texas Instruments, Inc.
//#############################################################################
// $TI Release: f2802x Support Library v200 $
// $Release Date: Tue Jul 24 10:01:39 CDT 2012 $
//#############################################################################

#include "DSP28x_Project.h" // Device Headerfile and Examples Include File

#include "f2802x_common/include/adc.h"
#include "f2802x_common/include/clk.h"
#include "f2802x_common/include/flash.h"
#include "f2802x_common/include/gpio.h"
#include "f2802x_common/include/pie.h"
#include "f2802x_common/include/pll.h"
#include "f2802x_common/include/spi.h"
#include "f2802x_common/include/wdog.h"

// Prototype statements for functions found within this file.
// interrupt void ISRTimer2(void);
void delay_loop(void);
void spi_xmit(uint16_t a);
void spi_fifo_init(void);
void spi_init(void);
void error(void);
void LCD_Init();
void delay_ms (Uint16 ms)
{
Uint16 i,j;
for(i=0;i<ms;i++) //外层循环若干毫秒
{
for(j=0;j<6000;j++); //内层循环1毫秒定时
}
}
void delay_us (Uint16 us)
{
Uint16 i,j;
for(i=0;i<us;i++) //外层循环若干微秒
{
for(j=0;j<60;j++); //内层循环1微秒定时
}
}


ADC_Handle myAdc;
CLK_Handle myClk;
FLASH_Handle myFlash;
GPIO_Handle myGpio;
PIE_Handle myPie;
SPI_Handle mySpi;

void main(void)
{
uint16_t sdata; // send data
uint16_t rdata; // received data

CPU_Handle myCpu;
PLL_Handle myPll;
WDOG_Handle myWDog;

// Initialize all the handles needed for this application
myAdc = ADC_init((void *)ADC_BASE_ADDR, sizeof(ADC_Obj));
myClk = CLK_init((void *)CLK_BASE_ADDR, sizeof(CLK_Obj));
myCpu = CPU_init((void *)NULL, sizeof(CPU_Obj));
myFlash = FLASH_init((void *)FLASH_BASE_ADDR, sizeof(FLASH_Obj));
myGpio = GPIO_init((void *)GPIO_BASE_ADDR, sizeof(GPIO_Obj));
myPie = PIE_init((void *)PIE_BASE_ADDR, sizeof(PIE_Obj));
myPll = PLL_init((void *)PLL_BASE_ADDR, sizeof(PLL_Obj));
mySpi = SPI_init((void *)SPIA_BASE_ADDR, sizeof(SPI_Obj));
myWDog = WDOG_init((void *)WDOG_BASE_ADDR, sizeof(WDOG_Obj));

// Perform basic system initialization
WDOG_disable(myWDog);
CLK_enableAdcClock(myClk);
(*Device_cal)();

//Select the internal oscillator 1 as the clock source
CLK_setOscSrc(myClk, CLK_OscSrc_Internal);

// Setup the PLL for x10 /2 which will yield 50Mhz = 10Mhz * 10 / 2
PLL_setup(myPll, PLL_Multiplier_10, PLL_DivideSelect_ClkIn_by_2);

// Disable the PIE and all interrupts
PIE_disable(myPie);
PIE_disableAllInts(myPie);
CPU_disableGlobalInts(myCpu);
CPU_clearIntFlags(myCpu);

// If running from flash copy RAM only functions to RAM
#ifdef _FLASH
memcpy(&RamfuncsRunStart, &RamfuncsLoadStart, (size_t)&RamfuncsLoadSize);
#endif

// Initalize GPIO
GPIO_setPullUp(myGpio, GPIO_Number_16, GPIO_PullUp_Enable);
GPIO_setPullUp(myGpio, GPIO_Number_18, GPIO_PullUp_Enable);

GPIO_setQualification(myGpio, GPIO_Number_16, GPIO_Qual_ASync);
GPIO_setQualification(myGpio, GPIO_Number_18, GPIO_Qual_ASync);

GPIO_setMode(myGpio, GPIO_Number_16, GPIO_16_Mode_SPISIMOA);
GPIO_setMode(myGpio, GPIO_Number_18, GPIO_18_Mode_SPICLKA);
//GPIO_setMode(myGpio, GPIO_Number_0, GPIO_0_Mode_GeneralPurpose);
//GPIO_setDirection(myGpio, GPIO_Number_0, GPIO_Direction_Output);
//GPIO_setLow(myGpio, GPIO_Number_0);


// GPIO_setMode(myGpio, GPIO_Number_19, GPIO_19_Mode_SPISTEA_NOT);

// Setup a debug vector table and enable the PIE
PIE_setDebugIntVectorTable(myPie);
PIE_enable(myPie);

spi_init(); // Initialize SPI
spi_fifo_init(); // Initialize the SPI FIFOs
LCD_Init(); //液晶初始化
//sdata = 0x0000;


// Transmit data
SPI_write(mySpi, 0xfa);
SPI_write(mySpi, 0x00);
SPI_write(mySpi, 0x30);
SPI_write(mySpi, 0x50);



// Wait until data is received
//while(SPI_getRxFifoStatus(mySpi) == SPI_FifoStatus_Empty){
//}

// Check against sent data
//rdata = SPI_read(mySpi);
//if(rdata != sdata)
// error();

//sdata++;

}


void delay_loop()
{
long i;

for (i = 0; i < 1000000; i++) {
}

return;
}

void error(void)
{
asm(" ESTOP0"); // Test failed!! Stop!
for (;;){
}
}

void spi_init()
{
CLK_enableSpiaClock(myClk);

// Reset on, rising edge, 16-bit char bits
SPI_setCharLength(mySpi, SPI_CharLength_8_Bits);

// Enable master mode, normal phase,
// enable talk, and SPI int disabled.
SPI_setMode(mySpi, SPI_Mode_Master);
SPI_enableTx(mySpi);

// SPI_setBaudRate(mySpi, SPI_BaudRate_500_KBaud);
SpiaRegs.***.all=0x007F;
// Relinquish SPI from Reset
SPI_enableLoopBack(mySpi);
SPI_enable(mySpi);

// Set so breakpoints don't disturb xmission
SPI_setPriority(mySpi, SPI_Priority_FreeRun);

return;
}

void spi_fifo_init()
{

// Initialize SPI FIFO registers
SPI_enableChannels(mySpi);
SPI_enableFifoEnh(mySpi);
SPI_resetTxFifo(mySpi);
SPI_clearTxFifoInt(mySpi);
SPI_resetRxFifo(mySpi);
SPI_clearRxFifoInt(mySpi);
SPI_setRxFifoIntLevel(mySpi, SPI_FifoLevel_4_Words);

return;
}

void LCD_Init()
{ delay_us(100);
SPI_write(mySpi, 0xf8);

SPI_write(mySpi, 0x30);//设置8位数据接口,基本指令模式

SPI_write(mySpi, 0x00);

SPI_write(mySpi, 0xf8);

SPI_write(mySpi, 0x00);//清DDRAM

SPI_write(mySpi, 0x20);

SPI_write(mySpi, 0xf8);

SPI_write(mySpi, 0x00);//游标及显示右移一位

SPI_write(mySpi, 0x60);

SPI_write(mySpi, 0xf8);

SPI_write(mySpi, 0x00);//整体显示开,游标关,反白光

SPI_write(mySpi, 0xC0);

SPI_write(mySpi, 0xf8);

SPI_write(mySpi, 0x00);//写入空格清屏幕

SPI_write(mySpi, 0x10);

SPI_write(mySpi, 0xf8);

SPI_write(mySpi, 0x00);//设定首次显示位置

SPI_write(mySpi, 0x10);

}
//===========================================================================
// No more.
//===========================================================================