This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LAUNCHXL-F280025C: 關於CAN bus receive data的DLC

Part Number: LAUNCHXL-F280025C


我參考範例”can_ex5_simple_receive”, 

裡面說到: Message Data Length: "Don't care" for a Receive mailbox,

但我需要知道receive data的DLC, 請問要如何得到?

  • 您好,我已向资深工程师寻求帮助。有了结果我会第一时间回复。

  • 以下函数可用于使用 IFx 寄存器读取 DLC 字段:

    //*****************************************************************************
    //
    // CAN_readMessageWithDLC
    //
    //*****************************************************************************
    bool CAN_readMessageWithDLC(uint32_t base,
                               uint32_t objID,
                               uint16_t *msgData,
                               uint16_t *msgLen)
    {
        bool status;
    
        //
        // Check the pointers.
        //
        ASSERT(msgLen != 0U);
    
        //
        //Read the message first this fills the IF2 registers
        //with received message for that mailbox
        //
        status = CAN_readMessage(base, objID, msgData);
        //
        // See if there is new data available.
        //
        if(status == true)
        {
            *msgLen = (HWREG_BP(base + CAN_O_IF2MCTL) & CAN_IF2MCTL_DLC_M);
        }
    
        return(status);
    }