Part Number: TMS320F28069M
您好,
我这有 typhoon设备与 28069M 连接, 但 28069输出的是 PWM信号。 但,我想让28069作为控制器,输出连续的控制量, 如-10到100范围内的数,而不是 0和1组成的PWM信号,请问我该怎么办,谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TMS320F28069M
您好,
我这有 typhoon设备与 28069M 连接, 但 28069输出的是 PWM信号。 但,我想让28069作为控制器,输出连续的控制量, 如-10到100范围内的数,而不是 0和1组成的PWM信号,请问我该怎么办,谢谢!
您好,看一下spruh18i_TMS320x2806x Microcontrollers Technical Reference Manual (Rev. I)的4.2.5.2 Implementing a DAC Function Using an R+C Reconstruction Filter
您好,请问, 我在CCS中算出的连续的控制量,怎么由28069m板卡输出呢?或者说, 28069m只能输出PWM信号吗?谢谢
您好,
在CCS中计算得到的连续数字量,从28069M的引脚能直接输出这些数字量吗?如-10 到 100 这些 数字量, 能否由28069直接输出?
是的,没有模拟输出。只能通过PWM加外部电路来实现,具体实现方式请参考我上面提到的TRM中的章节。
您好,谢谢,
请问 有数字输出吗, 能输出0, 1, 2, 3,4, 5,到 100,这些数字量吗? 谢谢