This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F2812: 请教时钟问题!

Part Number: TMS320F2812

请教专家:我在调试F2812,设置PLLCR=0xA;,但经常没有起作用,输出频率是晶振频率30M,只能反复断电复位,才可以到150M,也设置过PLLCR=0x8;,输出仍然是30M.

  • 您好,您有使用sysctrl.c中TI提供的函数去改变PLL吗?

    Fullscreen
    1
    2
    3
    4
    5
    6
    7
    8
    9
    10
    11
    12
    13
    14
    15
    16
    17
    18
    19
    20
    21
    EALLOW;
    SysCtrlRegs.PLLCR.bit.DIV = val;
    EDIS;
    // Optional: Wait for PLL to lock.
    // During this time the CPU will switch to OSCCLK/2 until the PLL is
    // stable. Once the PLL is stable the CPU will switch to the new PLL value.
    //
    // This switch time is 131072 CLKIN cycles as of Rev C silicon.
    //
    // Code is not required to sit and wait for the PLL to lock.
    // However, if the code does anything that is timing critical,
    // and requires the correct clock be locked, then it is best to
    // wait until this switching has completed.
    // If this function is run from waitstated memory, then the loop count can
    // be reduced as long as the minimum switch time is still met.
    // iVol is volatile so the compiler will not optimize this loop out
    //
    // The watchdog should be disabled before this loop, or fed within
    XXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXX

    这里需要wait time,并且在此期间需要禁用看门狗,这样就不会reset。

    如果您按照上述步骤,在一个步骤之内将您的系统从30MHz配置到150MHz可能会碰到一个问题。如果发生上述变化时芯片无法满足其浪涌电流需求,则可能会导致这种情况。一个解决方案是逐步增加PLL以逐渐增加电流负载,直到150MHz。

  • :谢谢您的指导!在设置PLLCR之前,我已经禁用了看门狗,也尝试分3次设置PLLCR(2、4、8),但仍然是30M。也不是说每次PLL都不奏效,很随机,但很多时间是不奏效的,一旦奏效,就能一直保持,即使复位,也依然能保持倍频,请指导!F2812,有人提到Xp_PLLDIS管脚需要上拉,如果上拉,上电后,CCS提示故障,根本无法进入到工作状态。DATAsheet,1.9V供电才可以到150M,1.8V只能到到135M,我尝试降低倍频,但也未奏效,写入FLASH后执行,基本没有问题,只是在调试时,不能倍频,谢谢,请指教!

  • 有人提到Xp_PLLDIS管脚需要上拉,如果上拉,上电后,CCS提示故障,根本无法进入到工作状态。

    如果在复位期间XPLLDIS引脚被拉低,则会禁用PLL。具体报错是什么?

    其余问题我需要和相关工程师讨论一下。

  • Yale Li:谢谢!根据您的建议,我对xPLLDIS引脚作上拉,上电,未出现上次故障,多次测试后可以倍频。虽有疑问,但也算是有一个解决办法,再次感谢您的帮助!

x 出现错误。请重试或与管理员联系。