This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

F28M35 TI-RTOS移植的疑问



您好!我在CCS下安装了TI-RTOS,展开可以先找到F28M35H52C1,然后里面不就有很多的例子,这些例子我该怎么用?

我现在说下我的理解,也就是实现移植的步骤,不对的地方请指出来。

1、建立C28和M3的工程。

2、拷贝CCS/TI-RTOS/F28M35H52C1下的一个例子到M3的工程中。

3、对工程进行修改。工程中的文件除了配置文件.cfg和main.c其他的都无需修改(还有哪些要修改吗?比如.h等头文件都不要修改了吧)。在配置文件中根据项目的需要,添加任务、变量等等。main函数中首先实现初始化(即完成时钟、管脚复用的配置)。然后其他的应用比如TCP/IP、usb等以任务来添加(可以另外一个.C的文件添加吗?即不同的任务建立一个.c文件,这样程序清晰些)。

这个思路步骤中间少了或是错了哪些吗?希望能指出来。

谢谢您的帮助!